Brewery cuts water usage by over a third
Improved monitoring helps Bath Ales reduce consumption
Bath Ales approached Endress+Hauser for help after realising that their water usage at the Hare Brewery near Bristol was too high. Without any means of monitoring where the water was being lost, there was no way to make efficiency improvements. A solution involving flowmeters, data collection panels and eSight software has resulted in impressive savings, bringing the ratio of water used as a proportion of the end product down from 8:1 to 5:1.
The benefits
-
Cost savings from reducing the volume of water used.
-
Environmental benefits of using less water.
-
Better overview of the process.
-
Potential to drive down the water usage even further and monitor other services using the same software.
The Challenge
As a key ingredient in beer and an essential component in a range of production processes, water is the lifeblood of breweries. Reducing the volume of water used in production along with any resulting wastewater is an important concern for all brewers, both to save money and to reduce the environmental impact of the business. Bath Ales, owned by Cornwall’s St Austell Brewery, were keen to reduce water usage at their newest facility, Hare Brewery near Bristol.
The solution
Endress+Hauser recommended a cost-effective solution: a high-accuracy Promag W400 flowmeter to be installed at the mains water inlet to the brewery as well as 12 lower-cost flowmeters for submetering. In addition, data collection panels were installed to capture the information from the flowmeters and automatically upload into the cloud-based software program eSight, which provides continuous monitoring and reporting of performance to baseline targets.
Impressive savings
The solution has brought the ratio of water used as a proportion of the end product down from 8:1 to 5:1, meaning that five pints of water instead of eight are now needed for every pint of beer produced. “By working with us to achieve our vision within budget, Endress+Hauser was certainly key to the understanding of the overall project and making sure that at the end of it we could deliver the reductions that we were hoping to see,” says Matt Newman.
Kontakt oss
Er du interessert i tilbudet vårt? Vil du diskutere bruksområdet ditt?
-
Standardprodukter
- Pålitelige, robuste og lette å vedlikeholde
Tekniske egenskaper
Enkelhet
-
Spesialprodukter
- Designet for krevende applikasjoner
Tekniske egenskaper
Enkelhet
Varierende
| FLEX utvalget | Tekniske egenskaper | Enkelhet |
|---|---|---|
Fundamental utvalg Møter dine grunleggende målebehov |
Tekniske egenskaper
|
Enkelhet
|
Lean utvalg Håndter henkelt dine kjerneprosesser |
Tekniske egenskaper
|
Enkelhet
|
Extended utvalg Optimaliser prosessene dine med innovative teknologier |
Tekniske egenskaper
|
Enkelhet
|
Xpert utvalg Mestre de mest utfordrende applikasjonene dine |
Tekniske egenskaper
|
Enkelhet
Varierende |