Title

Prøv å søke etter stikkord, ordre- eller produktkode eller serienummer, f.eks. “CM442” eller “teknisk informasjon”
Du må skrive inn minst 2 tegn for å starte søket.

Raman upstream bioprocess control

Nicro delivers turnkey fermentation systems with real-time metabolite and biomass monitoring

Industri: Livsvitenskap
Rxn-45 probe, bioprocess manufacturing, real-time, cGMP, COP/SIP, large-scale bioprocesses

Sammendrag

Nicro combined fermentation system engineering with Endress+Hauser Raman technology and analytical services from BICRO BIOCentre to create a complete solution for fermentation processes. Inline monitoring replaces time-consuming offline analysis with real-time measurements of metabolites and biomass. This gives scientists greater process insight, supports timely intervention, reduces contamination risk, and enables optimized production and increased yield.

The results: Faster, safer, and more productive fermentation

35

fermentation processes reached return on investment

33%

potential productivity increase over a 10-day period

The original cost analysis estimated a return on investment after 35 fermentation processes when inline Raman monitoring was compared with offline sample testing. The analysis also determined that the faster turnaround of Raman-monitored fermentation could increase plant productivity by 33% over a 10-day period.

Real-time insight improves fermentation control

Direct inline measurement of glycerol as an input metabolite, acetate as a byproduct, and OD600 for biomass growth provides deeper insight into fermentation performance. By monitoring multiple attributes through a single probe, the solution enables process decisions to be based on current conditions rather than delayed laboratory results. Results include:

  • Faster process cycle times through real-time metabolite monitoring
  • Improved process control supporting optimized production and increased yield
  • Reduced contamination risk by limiting offline sample handling
  • Simultaneous monitoring of multiple fermentation parameters
  • Reduced time between batches
  • A complete packaged technology solution for fermentation processes
Photo of Maja Marinović, PhD, Head of Microbiology Laboratory, BICRO BIOCentre Ltd

“Metabolic switch does not occur always at the same time, and online monitoring is the only way to know when exactly to intervene.”

Maja Marinović, PhD, Head of Microbiology Laboratory, BICRO BIOCentre Ltd

The challenge: Replace slow and risky offline analysis

Fermentation progress can be estimated by monitoring dissolved oxygen in the media. Optical density and metabolite concentrations provide additional insight, but these parameters have traditionally been measured offline using time-consuming chromatographic techniques.

Removing samples for analysis delays access to process information and introduces additional handling. It can also create a risk of contamination and the potential loss of a valuable batch. Nicro needed a solution that would provide timely information about metabolite concentration and biomass growth without relying on repeated offline sampling.

Our solution: Integrated Raman monitoring for fermentation

Nicro combined its fermentation engineering expertise with BICRO BIOCentre and Endress+Hauser technologies and services to provide a complete packaged solution for fermentation processes. The solution includes:

  • Engineering and design of a complete fermentation system from Nicro
  • An Endress+Hauser Raman Rxn analyzer
  • An Endress+Hauser Raman Rxn-45 probe
  • Analytical services from BICRO BIOCentre
  • S-PACT modeling services supporting analytical model development

The Raman probe is installed directly inline and monitors glycerol concentration, acetate concentration, and OD600 for biomass growth. Multiple attributes can be monitored simultaneously through one probe, providing a real-time view of fermentation conditions and eliminating the delay associated with offline sample analysis.

Inline information also helps scientists recognize process events that may not occur at exactly the same point in every batch. In the documented application, online monitoring allowed scientists to identify when bacteria switched from one carbon source to another, supporting intervention at the appropriate feed point.

Download the full case study

Want access to the full case study as a PDF?

Download a copy to read at your convenience, save for future reference, or share with colleagues.

Download the full case study

Kontakt oss

Er du interessert i tilbudet vårt? Vil du diskutere bruksområdet ditt?

Vær vennlig og gi oss så mange opplysninger som mulig så vi kan hjelpe deg på best mulig måte.

Products and services used

/

Related solutions and technology

Optisk analyse av kjemiske egenskaper

Optiske analysesystemer for overvåkning av kjemisk sammensetning og konsentrasjon i gass, væsker og faststoffer – for laboratorie-, prosess- og utslippsovervåking.

Mer informasjon

Overvåking av avløpsutslipp 

Håndter utslipp av avløpsvann innenfor lovlige grenser med fullstendig og pålitelig overvåking av kontinuerlige verdier og rask respons på forurensning.

Les mer

Hydrogenmåling i naturgassrørledninger

Rask, kontinuerlig måling av hydrogen i naturgassrørledninger muliggjør sikker blanding, etterlevelse av kvalitetskrav og dynamisk styring ved hjelp av Raman-spektroskopi – uten forbruksvarer eller fakling

Les mer

Kvalitetsanalyse av biometan for sikker og regelverksmessig gassinjeksjon 

Sikre pålitelig biometankvalitet med rask, nøyaktig nettbasert måling av H₂S, vannets duggpunkt og kritiske parametere for sikker innmating i nettet og effektiv drift. 

Les mer

Beskytt omvendt osmose-membraner med nettbasert overvåking av vannkvaliteten ved avsalting 

Pålitelig nettbasert overvåking av vannkvaliteten for å beskytte RO-membraner (omvendt osmose), redusere rengjøringsarbeidet og forlenge membranenes levetid i avsaltings- og vanngjenbruksbruksområder

Les mer

Påvisning av lekkasjer i kryogene tanker (LNG, etylen, LPG og ammoniakk)

Oppdag lekkasjer i kryogentanker tidlig og behold kontrollen. Endress+Hauser tilbyr kontinuerlig og svært pålitelig temperaturovervåkning for å beskytte mennesker, eiendeler og kritisk infrastruktur.

Les mer

CCUS-måling og verifisering i sanntid

Åpne for fremtiden innen karbonfangst: presis, pålitelig og skreddersydd for tettfaseapplikasjoner

Les mer

Løsninger for kontinuerlig utslippsovervåking for å sikre overholdelse

Løsninger for kontinuerlig utslippsovervåking for å sikre overholdelse

Mer informasjon

FAQs

Firmalogo av: Nicro

Nicro is a Croatian company whose tailored bioreactors propelled the rise of pharma, biotech, food and chemical industries in the region.