Title

Prøv å søke etter stikkord, ordre- eller produktkode eller serienummer, f.eks. “CM442” eller “teknisk informasjon”
Du må skrive inn minst 2 tegn for å starte søket.

Reliable compliance with limit values

Demand-oriented dosing saves up to 40% of precipitent

Together with Endress+Hauser, Veolia Wasser Deutschland GmbH has developed a solution for the demand-oriented and automated precipitent dosing in the aeration basins of the wastewater treatment plant in Colditz.

Discover how sustainable wastewater management can be achieved

Collaboration between Veolia and Endress+Hauser ©Endress+Hauser

Collaboration between Veolia and Endress+Hauser

Results

  • Reliable compliance with legal limits for orthophosphate

  • Precise dosing of the precipitent according to requirements

  • Reduced operating costs

  • Increased operational reliability through remote access

  • Fast response times in case of disruption

Martin Moisel

“Endress+Hauser helped us to obtain the values promptly so that the precipitent dosage was not over- or underdosed.”

Martin Moisel, Head of Operations / Technical Manager
Veolia Wasser Deutschland

Customer challenge

Compliance with legally prescribed limit values for orthophosphate posed a number of challenges for the wastewater treatment plant in Colditz. Previously, the precipitent was dosed on the basis of weekly laboratory analyses – however, these only provided selective results and were unable to record fluctuations depending on the time of day or week. Continuous and more precise monitoring of the phosphate content was necessary in order to meet the increasing requirements in the long term.

Our solutions

Endress+Hauser partnered with Veolia to implement continuous phosphate monitoring using the CA80PH analyzer. It measures phosphate levels in two aeration basins, enabling precise dosing of precipitent.
Digital technologies were also used: The measurement data is transmitted in real time via the Netilion Cloud. This allows maintenance requirements to be recognized immediately. Thanks to additional remote access, the Endress+Hauser service team can access the analyzer directly.

Kontakt oss

Er du interessert i tilbudet vårt? Vil du diskutere bruksområdet ditt?